3.3 Batch Files
Since multiple commands are executed to perform various operations pertaining to calibration, typing individual commands manually is a tedious process. Batch files are therefore used to automate the process. Based on the programming tool and interface used, the batch file naming convention is:
atprogram_<toolname>_<interface>_rc_calib.bat
Example: atprogram_ATMELICE_ISP_rc_calib.bat
If the tool used is JTAGICE3 and interface is JTAG, for example, the file name would be:
atprogram_JTAGICE3_JTAG_rc_calib.bat