6.2.1.1 rlm startup options
The rlm command is:
% rlm [-c license_file] [-dat] [-dlog [+]logfile] [-iai] [-info]
[-l] [-noudp] [-nows | -ws port] [-x [rlmdown|rlmremove]]
[-install_service] [-service_name sname]
[-v] [-user username -password password]
[-isv_startup_delay seconds]
The -c license_file
option specifies which license file to use. This option overrides the setting of the RLM_LICENSE environment variable. The license_file
parameter can be a directory containing license files, all of which will be processed.
The -dat
option specifies that license files should have the extension “.dat”, rather than “.lic”. If -dat
is specified, the rlm server will search for all files ending in “.dat” instead of “.lic” as documented elsewhere.
The -dlog logfile
specifies the pathname for the server debug log. If logfile
is preceded by the '+' character, the logfile will be appended, otherwise it is overwritten.
The -iai
switch specifies that the server should run even though the user
running it is root or an admin user. When running in this mode, the webserver will be
disabled. (v14.1+)
The -info
option causes RLM to print information about all copies of rlm that are running on this computer, including copies which have run in the prior 24 hours, then exit.
The -install_service
and -service_name sname
options are used to run the rlm server as a service under Windows. See the description of running the rlm server as a service below.
Notes on using the -user and -password options:
- Windows expects the
username
argument to be <domain>\<user>. To use the local system domain, specify ".\<username>", eg ".\joe". Without the ".\" you will get a service creation failure. - In order to run a service, the account specified by the
-user
argument must have the "Log on as a Service" property set. For details on how to set that property on an account, see this blog:
The -isv_startup_delay seconds
option specifies that when running as a Windows service, rlm should delay seconds seconds before starting up the ISV servers. If not specified, there is no delay. This is useful if a license file specifies a hostid of type rlmid1 or rlmid2 (hardware keys), the server is started at system boot time, and the key driver is not yet started at the time the ISV server needs to read it.
The -nows
and -ws port
options control the operation of the embedded Web Server. The -nows
option instructs the rlm server to not start the embedded web server. The -ws port
option instructs the rlm server to use port as the port number for the web server.
The -noudp
option tells RLM to not bind the UDP port (5053) used for replying to broadcast messages from clients in RLM v10.0 and later. This option is not used by Microchip.
The -v
option causes RLM to print it's version and exit.
The -x [rlmdown | rlmremove]
option controls whether the rlmdown and/or rlmremove commands will be processed by the server. Specifying only -x
will disable both commands. Specifying either command name after the -x
will disable just that command.
These options can appear in any order on the command line.
If you want to generate a report log file, specify this on an ISV-by-ISV basis in the individual ISV's options file. See the description of the REPORTLOG line in The ISV Options File for more information.
Note that if the rlm
server cannot bind the web server port (5054 by default), it will exit.
If the ISV server pathname is incorrect in a license file which RLM is processing, RLM will attempt to start that ISV server using the path information in other license files, if present.