3.1 Starting the License Server
To start the network license server, you need to have a Command or Terminal window open to the bin directory in the path that you selected to install the license server.
You will also need to know where the license files were installed. You can find this out
by running, in the bin
directory, xclm
-licensepath
.
You start the license server by running:
rlm -c <license path>
where rlm
is the RLM license server and -c
is the
option to specify the directory that holds the license files, <license
path>
.
This starts the server and displays the log in the window. You must keep this window open so that the server will continue to run. If you need to have the server automatically run, please see the next section.
Running Server
> rlm -c C:\ProgramData\Microchip\xclm\license
04/22 23:55 (rlm) RLM License Server Version 14.1BL3
Copyright (C) 2006-2020, Reprise Software, Inc. All rights reserved.
04/22 23:55 (rlm) License server started on PAWS-BOX
04/22 23:55 (rlm) Server architecture: x64_w4
04/22 23:55 (rlm) License files:
04/22 23:55 (rlm) C:\ProgramData\Microchip\xclm\license\microchip-1.lic
04/22 23:55 (rlm) C:\ProgramData\Microchip\xclm\license\microchip-2.lic
04/22 23:55 (rlm) C:\ProgramData\Microchip\xclm\license\microchip-3.lic
04/22 23:55 (rlm)
04/22 23:55 (rlm) Using options file rlm.opt
04/22 23:55 (rlm) Web server starting on port 5054
04/22 23:55 (rlm) Using TCP/IP port 5053
04/22 23:55 (rlm) ... adding UDP/IP port 5053
04/22 23:55 (rlm) Starting ISV server microchip on port 54765
04/22 23:55 (rlm) New thread created to watch ISV microchip
04/22 23:55 (microchip) RLM License Server Version 14.1BL3 for ISV "microchip"
04/22 23:55 (microchip) Settings from RLM Version 14.1BL3 for ISV "microchip"
04/22 23:55 (microchip) Server architecture: x64_w4
Copyright (C) 2006-2020, Reprise Software, Inc. All rights reserved.
RLM contains software developed by the OpenSSL Project
for use in the OpenSSL Toolkit (http://www.openssl.org)
Copyright (c) 1998-2008 The OpenSSL Project. All rights reserved.
Copyright (c) 1995-1998 Eric Young (eay@cryptsoft.com) All rights reserved.
04/22 23:55 (microchip)
04/22 23:55 (microchip) Server started on PAWS-BOX (hostid: 2c44fd110393) for:
04/22 23:55 (microchip) swxc8n-pro swxc16n-pro swxc32n-pro
04/22 23:55 (microchip)
04/22 23:55 (microchip) License files:
04/22 23:55 (microchip) C:\ProgramData\Microchip\xclm\license\microchip-1.lic
04/22 23:55 (microchip) C:\ProgramData\Microchip\xclm\license\microchip-2.lic
04/22 23:55 (microchip) C:\ProgramData\Microchip\xclm\license\microchip-3.lic
04/22 23:55 (microchip)