5.3 Restrict the hostIDs that can use a license

Create an option file called microchip.opt in the same location as the license files and add the following lines to the file:

HOST_GROUP project_group <hostname> <another_hostname> …

INCLUDE product_name host_group project_group

where product_name represents values found in 5.9 Determine the Product Name. This must be the same as the second value after the LICENSE in the license file:

LICENSE microchip product_name permanent 24 …

Include all the hostnames (computer names) for the client computers to which you wish to be able to use the license.

See also 6.2.7 The ISV Options File.