5.5 Set the maximum roaming interval
The default maximum number of days a license can be roamed out is 30 before the license is automatically returned. You can specify a shorter interval, but 30 is the absolute maximum.
Create an option file called microchip.opt in the same location as the
license files and add the following line to the file:
ROAM_MAX_DAYS 14 product_name
where product_name represents values found in 5.9 Determine the Product Name.
This line limits the number of days that an MPLAB XC C compiler Pro license that can roam to 14.
The last value on the ROAM_MAX_DAYS is the product and must be the same
as the third value of the LICENSE line in the license file:
LICENSE microchip product_name permanent 24 …
See also 6.2.7 The ISV Options File.