2.1.3.2 DIAG_WDT_GetRSTFRCopy()

uint8_t DIAG_WDT_GetRSTFRCopy (void )

Returns the copy/backup of the RSTFR register.

This API should be called in main after performing the DIAG_WDT_Startup diagnostic to ensure that the reset reason is handled by the application. It is required because the DIAG_WDT_Startup diagnostic clears the RSTFR register.
Parameters:
None.
Returns:

Copy of Reset Flag register (RSTFR) or DIAG_RSTFR_COPY_INVALID if the backup in SRAM has been corrupted.