1 Harmony 3 Driver and System Service Application Examples for PIC32MZ W1 Family
The following applications are provided to demonstrate the typical or interesting usage models of one or more drivers and system services.
Name | Description |
---|---|
Console Debug System Service using UART | This example application demonstrates the UART based console and debug system service |
Console Debug System Service using USB | This example application demonstrates the USB based console and debug system service |
FAT Filesystem using NVM Media | This application shows an example of implementing a FAT disk in the device internal Flash memory |
FAT Filesystem using SD Card Media | This application shows an example of using the MPLAB Harmony File System to access and modify the contents of a SD card using the SDSPI driver and the SPI PLIB |
FAT Filesystem using SST26 Media | This application shows an example of using the FAT File System to access SST26 flash media using SPI protocol |
FreeRTOS Basic | This example application demonstrates context switching between four tasks of different priorities. Two tasks run periodically while the other two tasks are event driven |
I2C Driver Asynchronous - I2C EEPROM | This example application shows how to use the I2C driver in asynchronous mode to perform operations on the EEPROM |
I2C Driver Synchronous - I2C EEPROM | This example application shows how to use the I2C driver in synchronous mode to perform operations on the EEPROM |
LittleFS Filesystem using NVM Media | This application shows an example of implementing a LittleFS disk in the device internal Flash memory |
LittleFS Filesystem using SST26 Media | This application shows an example of using the LittleFS File System to access SST26 flash media using SPI protocol |
SPI Driver Asynchronous - Self Loopback Multi Client | This example demonstrates how to use the SPI driver in asynchronous mode to achieve self-loop back between multiple clients |
SPI Driver Synchronous - Self Loopback Multi Client | This example demonstrates how to use the SPI driver in synchronous mode to achieve self-loop back between multiple clients in RTOS environment |
Time System Service Multi-client | This example application demonstrates the multi-client system timer functionality |
USART Driver Asynchronous - USART Echo | This example echoes the received characters over the console using the USART driver in asynchronous mode |
USART Driver Synchronous - USART Echo | This example echoes the received characters over the console using the USART driver in synchronous mode |