1.8 I2C Driver Synchronous - I2C EEPROM
This example application shows how to use the I2C driver in synchronous mode to perform operations on the EEPROM.
Description
This example uses the I2C driver in synchronous mode to communicate with the EEPROM to perform write and read operations in Bare-Metal environment. This application uses I2C driver to read and write data from an AT24CM02 EEPROM device.
Downloading and Building the Application
To clone or download this application from Github, go to the main page of this repository and then click Clone button to clone this repository or download as zip file. This content can also be downloaded using content manager by following these instructions.
Path of the application within the repository is apps/driver/i2c/sync/i2c_eeprom/firmware.
To build the application, refer to the following table and open the project using its IDE.
Project Name | Description |
---|---|
pic32mz_w1_curiosity_freertos.X | MPLABX project for PIC32MZ W1 Curiosity Board |
Setting Up the Hardware
The following table shows the target hardware for the application projects.
Project Name | Description |
---|---|
pic32mz_w1_curiosity_freertos.X | PIC32MZ W1 Curiosity Board |
- To run the demo, the following additional hardware are required:
- One EEPROM 3 Click board
Setting Up PIC32MZ W1 Curiosity Board
- Connect micro USB cable to the ‘USB Debug’ connector(J302) on the board to the computer
- Install the EEPROM 3 Click board on to the mikroBUS socket J200 of PIC32MZ W1 Curiosity Development Board
Running the Application
- Build and program the application using its IDE
- The LED is turned ON when the value read from the EEPROM matched with the written value
Board | LED Name |
---|---|
PIC32MZ W1 Curiosity Board | RED LED |