2.2.2 USR_MLME_ResetConf callback Function
C
void USR_MLME_ResetConf(uint8_t status)Summary
Callback function that must be implemented by application (NHLE) for MAC service MLME-RESET.confirm.
Description
This function implemented by application (NHLE) for MAC service MLME-RESET.confirm.
Precondition
WPAN_Init() should have been called before calling this function.
Parameters
| Param | Description |
|---|---|
| status | Result of requested reset operation |
Returns
None.
Example
void USR_MLME_ResetConf(uint8_t status)
{
status = status;
}
Remarks
There is weak function for this callback. User has to define own implementation for required operation on the reception of particular callback.