2.14.1 WPAN_MLME_RxEnableReq Function
C
bool WPAN_MLME_RxEnableReq(bool DeferPermit, uint32_t RxOnTime, uint32_t RxOnDuration)Summary
Initiate MLME-RX-ENABLE.request service and have it placed in the MLME-SAP queue.
Description
This function is used by the NHLE layer to request that the receiver is either enabled for a finite period of time or disabled. It initiates MLME-RX-ENABLE.request service and have it placed in the MLME-SAP queue.
Precondition
WPAN_Init() should have been called before calling this function.
Parameters
| Param | Description |
|---|---|
| DeferPermit | Set to true if receiver enable can be deferred until next super frame if requested time has already passed |
| RxOnTime | Number of symbols from start of superframe before receiver |
| RxOnDuration | Number of symbols for which the receiver is enabled |
Returns
true - success; false - buffer not available or queue full.
Example
bool retVal = false; bool DeferPermit = true; uint32_t RxOnTime = 0x000000; uint32_t RxOnDuration = 100; retVal = WPAN_MLME_RxEnableReq(DeferPermit, RxOnTime, RxOnDuration); if (true != retVal) { printf("buffer not available or queue full"); }
Remarks
On the receipt of WPAN_MLME_RxEnableReq, MAC layer will perform respective operation and asynchronously invokes USR_MLME_RxEnableConf with proper status.