2.12.1 WPAN_MLME_OrphanResp Function
C
bool WPAN_MLME_OrphanResp(uint64_t OrphanAddress, uint16_t ShortAddress, bool AssociatedMember)Summary
Initiate MLME-ORPHAN.response service and have it placed in MLME_SAP queue.
Description
This function is used to allow the next higher layer of a coordinator to respond to the MLME-ORPHAN.indication primitive. It initiates MLME-ORPHAN.response service and have it placed in MLME_SAP queue. The MLME-ORPHAN.indication primitive allows the MLME of a coordinator to notify the next higher layer of the presence of an orphaned device.
Precondition
WPAN_Init() should have been called before calling this function.
Parameters
| Param | Description |
|---|---|
| OrphanAddress | Address of orphaned device |
| ShortAddress | Short address allocated to orphaned device |
| AssociatedMember | Boolean true if the orphaned device is associated |
Returns
true - success; false - buffer not available or queue full.
Example
uint64_t OrphanAddress = 0x0000111100001111; uint16_t shortaddr = 0x0001; bool retVal = false; retVal = WPAN_MLME_OrphanResp(OrphanAddress,shortaddr, true) if (true != retVal) { printf("buffer not available or queue full"); }
Remarks
On the receipt of WPAN_MLME_OrphanResp, MAC layer will perform respective operation and asynchronously invokes USR_MLME_CommStatusInd with proper status.