2.9.2 USR_MCPS_DataConf callback Function
C
void USR_MCPS_DataConf(uint8_t msduHandle, uint8_t status, uint32_t Timestamp)Summary
Callback function that must be implemented by application (NHLE) for MAC service MCPS-DATA.confirm.
Description
This function implemented by application (NHLE) for MAC service MCPS-DATA.confirm.
Precondition
WPAN_Init() should have been called before calling this function.
Parameters
| Param | Description |
|---|---|
| msduHandle | Handle of MSDU handed over to MAC earlier |
| status | Result for requested data transmission request |
| Timestamp | The time, in symbols, at which the data were transmitted, this parameter is only available if timestamping is enabled via compile switch ENABLE_TSTAMP |
Returns
None.
Example
USR_MCPS_DataConf(uint8_t msduHandle, uint8_t status, uint32_t Timestamp)
{
msduHandle = msduHandle;
status = status;
Timestamp = Timestamp;
}Remarks
There is weak function for this callback. User has to define own implementation for required operation on the reception of particular callback.