2.11.1 USR_MLME_BeaconNotifyInd callback Function
C
void USR_MLME_BeaconNotifyInd(uint8_t BSN, WPAN_Pandescriptor_t *PANDescriptor, uint8_t PendAddrSpec, uint8_t *AddrList, uint8_t sduLength, uint8_t *sdu);Summary
Callback function that must be implemented by application (NHLE) for MAC service MLME-BEACON-NOTIFY.indication.
Description
This function implemented by application (NHLE) for MAC service MLME-BEACON-NOTIFY.indication.
Precondition
WPAN_Init() should have been called before calling this function.
Parameters
| Param | Description |
|---|---|
| BSN | Beacon sequence number |
| PANDescriptor | Pointer to PAN descriptor for received beacon |
| PendAddrSpec | Pending address specification in received beacon |
| AddrList | List of addresses of devices the coordinator has pending data |
| sduLength | Length of beacon payload |
| sdu | Pointer to beacon payload |
Returns
None.
Example
void USR_MLME_BeaconNotifyInd(uint8_t BSN, WPAN_Pandescriptor_t *PANDescriptor, uint8_t PendAddrSpec, uint8_t *AddrList, uint8_t sduLength, uint8_t *sdu);
{
DeviceAddress = DeviceAddress;
CapabilityInformation = CapabilityInformation;
}Remarks
There is weak function for this callback. User has to define own implementation for required operation on the reception of particular callback.