2.7.3 USR_MLME_DisassociateInd callback Function
C
void USR_MLME_DisassociateInd(uint64_t DeviceAddress, uint8_t DisassociateReason)Summary
Callback function that must be implemented by application (NHLE) for MAC service MLME-DISASSOCIATE.indication.
Description
This function implemented by application (NHLE) for MAC service MLME-DISASSOCIATE.indication.
Precondition
WPAN_Init() should have been called before calling this function.
Parameters
| Param | Description |
|---|---|
| DeviceAddress | Extended address of device which initiated the disassociation request |
| DisassociateReason | Reason for the disassociation. Valid values: - @ref WPAN_DISASSOC_BYPARENT, - @ref WPAN_DISASSOC_BYCHILD |
Returns
None.
Example
void USR_MLME_DisassociateInd(uint64_t DeviceAddress, uint8_t DisassociateReason)
{
DeviceAddress = DeviceAddress;
DisassociateReason = DisassociateReason;
}
Remarks
There is weak function for this callback. User has to define own implementation for required operation on the reception of particular callback.