2.5.1 WPAN_MLME_StartReq Function
C
bool WPAN_MLME_StartReq(uint16_t PANId, uint8_t LogicalChannel, uint8_t ChannelPage, uint8_t BeaconOrder, uint8_t SuperframeOrder, bool PANCoordinator, bool BatteryLifeExtension, bool CoordRealignment)Summary
Initiate MLME-START service and have it placed in the MLME-SAP queue.
Description
This function is used by the PAN coordinator to initiate a new PAN. It initiates MLME-START service and have it placed in the MLME-SAP queue. The MLME-START.request primitive allows the PAN coordinator to initiate a new PAN or to begin using a new super frame configuration. This primitive may also be used by a device already associated with an existing PAN to begin using a new super frame configuration.
Precondition
WPAN_Init() should have been called before calling this function.
Parameters
| Param | Description |
|---|---|
| PANId | PAN identifier to be used by device |
| LogicalChannel | The logical channel on which to start using the new super frame configuration |
| ChannelPage | The channel page on which to begin using the new super frame configuration |
| SuperframeOrder | Duration of active portion of super frame |
| PANCoordinator | Indicates whether node is PAN coordinator of PAN |
| BatteryLifeExtension | Boolean true disables receiver of beaconing device |
| CoordRealignment | Boolean to transmit Coordinator Realignment command prior to changing to new super frame configuration |
Returns
true - success; false - buffer not available or queue full.
Example
bool retVal = false; uint8_t current_channel = 13; uint8_t current_channel_page = 0; uint16_t panid = 0x1111; uint8_t default_beacon_order = 15; uint8_t default_superframe_order = 15; retVal = WPAN_MLME_StartReq(panid, current_channel, current_channel_page, default_beacon_order, default_superframe_order, true, false, false); if (true != retVal) { printf("buffer not available or queue full"); }
Remarks
On the receipt of WPAN_MLME_StartReq, MAC layer will perform respective operation and asynchronously invokes USR_MLME_StartConf with proper status.