9.6.5 Example Project
In the following, an example project for SEGGER Embedded Studio can be downloaded that demonstrates:
- How to use monitor mode in Embedded Studio
- How to have a specific interrupt keep firing while the main application is halted and the monitor is active
For more detailed explanations how to bring the project up and running on a specific hardware, please refer to the readme that comes with the project.