4.2 Jumper Options

The CEC173x evaluation board has a variety of configuration jumpers.

The jumpers and headers have a J reference designator. Several of the jumpers have been replaced by a special trace-link PCB structure, in which the default value for the jumper is hardwired into the design. A representative picture of this PCB structure for jumper J23 is shown in the figure below, labeled “Trace-Link Jumper”. To change the value of these jumpers, the user must cut the default trace and install a resistor across the alternate connection pads. For instance, to change the configuration of J23, cut the trace between pins 1 and 2, and install a zero Ohm 0603 surface-mount resistor between pads 2 and 3. In some cases, jumpers have been replaced with a single 0 Ohm resistor. For these jumpers, the options are either installed (IN) or not installed (OUT). The resistors used in these locations are listed in Table 4-1. In other cases, a standard jumper cap must be placed across jumper pins in the default position for default operation of the device.

Figure 4-2. Trace-Link Jumper
The following table of jumpers is based on the original EV19K07A evaluation board. Where possible, original jumper names have been retained for consistency. A jumper type column was added to make it easy to identify what type of jumper is used. The following types are identified:
  1. Standard – A standard jumper uses a header and a jumper cap to modify the design.
  2. 0 Ohm Short – Instead of a selection jumper, one or more zero Ohm jumpers were used to replace the original jumper. The Configuration Options column indicates which resistors were used to replace the jumper.
  3. Trace-Link – A PCB structure that shorts through a direct metal link to the default position
  4. Header – Not a jumper, but a header to interface with the outside world.
  5. Removed – A jumper that existed on the original EV19K07A board but was removed from the EV42J24A board.
Important: The following table covers both revision 2 and revision 3 of the EV42J24A evaluation board. The jumper type and description columns provide data on both versions of the board when they differ.
Table 4-1. Jumper Options and Headers
JumperFunctionBoard Rev 2/3

Jumper Type

Configuration Options
J1Board Power SelectionStandard1-2: Power by external 5V Adapter (P1)

2-3 (Default): Power by micro-USB Port (P2, P3)

J2VTR power to CEC173x0 Ohm Short - R163IN (Default): Connect VTR power

OUT: Disconnect VTR power

J3+3.3V power to MEC17230 Ohm Short - R166IN (Default): Connect +3.3V power

OUT: Disconnect +3.3V power

J4VTR_PLL power to CEC173x0 Ohm Short - R164IN (Default): Connect VTR_PLL power

OUT: Disconnect VTR_PLL power

J5+1.8V power to MEC17230 Ohm Short - R167IN (Default): Connect +1.8V power

OUT: Disconnect +1.8V power

J6CEC173x I2C SCL selection to MCP2221AStandard1-2: I2C10

3-4 (Default): I2C06

5-6: I2C00

J7VTR_ANALOG power to CEC173x0 Ohm Short - R165IN (Default): Connect VTR_ANALOG power

OUT: Disconnect VTR_ANALOG power

J8+3.3V power to CEC173x0 Ohm Short - R168IN (Default): Connect +3.3V power

OUT: Disconnect +3.3V power

J9+1.8V power to CEC173x0 Ohm Short - R169IN (Default): Connect +1.8V power

OUT: Disconnect +1.8V power

J10VTR1 power selection for CEC173xStandard1-2 (Default): Connect +3.3V power

3-4: Connect +1.8V power

J11CEC173x I2C SDA selection to MCP2221AStandard1-2: I2C10

3-4 (Default): I2C06

5-6: I2C00

J12VTR2power selection for CEC173xStandard1-2 (Default): Connect +3.3V power

3-4: Connect +1.8V power

J13VTR_REG power to MEC17230 Ohm Short - R170IN (Default): Connect VTR_REG power

OUT: Disconnect VTR_REG power

J14VTR2 power selection for MEC1723Rev 2:

Trace-Link

Rev 2:

1-2 (Default): Connect +3.3V power

3-4: Connect +1.8V power

Rev 3:

Standard

Rev 3:

1-2 (Default): Connect +3.3V power

2-3: Connect +1.8V power

J15VTR_PLL power to MEC17230 Ohm Short - R173IN (Default): Connect VTR_PLL power

OUT: Disconnect VTR_PLL power

J16VTR_ANALOG power to MEC17230 Ohm Short - R175IN (Default): Connect VTR_ANALOG power

OUT: Disconnect VTR_ANALOG power

J17VTR1 power to MEC17230 Ohm Short - R176IN (Default): Connect VTR1 power

OUT: Disconnect VTR1 power

J18VBAT power to MEC17230 Ohm Short - R177IN (Default): Connect VBAT power

OUT: Disconnect VBAT power

J19VTR3 power to MEC17230 Ohm Short - R178IN (Default): Connect VTR3 power

OUT: Disconnect VTR3 power

J20CEC173x GPIO012/nEXTRST Pull selectionTrace-Link1-2 (Default): Pull-high to VTR_REG

2-3: Pull-down

J21CEC173x GPIO106/AP0_nRESET Pull selectionTrace-Link1-2 (Default): Pull-high to VTR_REG

2-3: Pull-down

J22CEC173x GPIOs HeaderHeaderFor debug purposes
J23CEC173x GPIO1316/AP1_nRESET Pull selectionTrace-Link1-2 (Default): Pull-high to VTR_REG

2-3: Pull-down

J24CEC173x nRESET_IN pinStandard1-2 (Default): Normal operation

2-3: Hold CEC1736 in reset

J25CEC173x JTAG _STRAP pinTrace-Link1-2: Put in boundary scan mode

2-3 (Default): Normal operation

J26CEC173x GPIO055 Strap OptionTrace-Link1-2 (Default)
J27CEC173x I2C_ADDR0 StrapTrace-Link1-2: Pull-high to VTR_REG

2-3 (Default): Pull-down

J28CEC173x CR_FLASH StrapTrace-Link1-2 (Default): Normal operation

2-3: Boot from crisis recovery Flash component

J29CEC173x GPIO124 Strap OptionTrace-Link1-2 (Default)
J30CEC173x BSTRAP StrapStandard1-2 (Default): Normal operation

2-3: Boot from I2C or UART Crisis Port

J31CEC173x I2C_ADDR1 StrapTrace-Link1-2: Pull-high to VTR_REG

2-3 (Default): Pull-down

J32CEC173x RESET_IN# Delay Circuit Power SourceTrace-Link1-2 (Default): Connect +3.3V power

2-3: Connect VTR_REG power

J33CEC173x PICKIT4 1x8 HeaderHeaderFor debug purposes
J34CEC173x 32KHz Single-End Source0 Ohm Short - R151IN (Default): Connect oscillator

OUT: Disconnect oscillator

J35CEC173x RESET_IN# delay circuit0 Ohm Short - R152R152 IN (Default): Connect delay circuit

OUT: Disconnect delay circuit

J36CEC173x GPIO157/LED1 & GPIO156/LED0 pins connection0 Ohm ShortR154 1-2 (Default): Connect GPIO157 to LED5

R155 3-4 (Default): Connect GPIO156 to LED6

J37CEC173x RESET_IN# pin ground0 Ohm Short - R153IN: Hold CEC1736 in Reset

OUT (Default): Normal operation

J38CEC173x UART0 debug headerStandardFor debug purposes
J39MEC1723 Test Clocks Out headerStandardFor debug purposes
J40MEC1723 32KHz Single-End Input selection (Optional)0 Ohm ShortUse R180, R181 and R67 to select the clock source
J41MEC1723 I2C02 channel headerStandardFor debug purposes
J42MEC1723 I2C07 channel headerStandardFor debug purposes
J43MEC1723 RESET_IN# delay circuitStandardIN: Connect delay circuit

OUT (Default): Disconnect delay circuit

J44MEC1723 RESET_IN# pin groundRev 2:

0 Ohm Short - R156

Closed: MEC1723 in reset

IN: Hold MEC1723 in reset

OUT (Default): Normal operation

Rev 3:

Standard

Rev 3:

Closed: MEC1723 held in reset

Open: MEC1723 not in reset. (Default)

J45MEC1723 PICKIT4 1x8 HeaderHeaderFor debug purposes
J46MEC1723 GPIO156/LED0, GPIO157/LED1, and GPIO153/LED2 pins connection0 Ohm ShortR140 (Default): Connect GPIO156 to LED9

R141 (Default): Connect GPIO157 to LED10

R142 (Default): Connect GPIO153 to LED11

J47CEC173x Bypass ModeRev 2:

Header

Rev 2:

Eliminated in this revision

Rev 3:

2-pin Header

Rev 3:

Closed: ByPass Mode

Open: (Default) Normal Operation

J48U8 SPI Flash power source selectionRemovedU8 and J48 eliminated in this revision
J49MEC1723 XTAL2 selectionTrace-Link1-2 (Default): Connect to 2-pin crystal

2-3: Connect to single-end 32 KHz source

J50MEC1723 XTAL1 selection0 Ohm Short - R159IN (Default): Connect to 2-pin crystal

OUT: Use single-end 32 KHz source, floating

J51U8 SPI Flash isolation jumperRemovedEliminated in this revision
J52MEC1723 JTAG _STRAP pinTrace-Link1-2: Put in boundary scan mode

2-3 (Default): Normal operation

J53MEC1723 CMP_STRAP pinTrace-Link1-2 (Default)
J54MEC1723 CR_STRAP pinTrace-Link1-2 (Default): Boot from SHD_SPI Flash via CEC1736

2-3: Boot from PVT_SPI Flash (U8)

J55MEC1723 UART0 debug headerStandardFor debug purposes
J56MEC1723 UART_BSTRAP pinTrace-Link1-2 (Default): Normal operation

2-3: Boot from UART Crisis Port

J57MEC1723 BSS_STRAP pinTrace-Link1-2 (Default): Normal operation

2-3: Not boot in this application

J58CEC173x QSPI0 CS0 Pass/Failure Cases selection for demonstration purposeRemovedEliminated in this revision
J59CEC173x Flash Bus 1 Power selectStandard1-2 (Default): Connect to board power

2-3: Connect DediProg power

J60CEC173x Flash Bus 2 Power selectStandard1-2 (Default): Connect to board power

2-3: Connect DediProg power

J61DediProg SPI Programming HeaderHeaderUse for U9 or U13 SPI Flash programming
J62DediProg SPI Programming HeaderHeaderUse for U10 or U12 SPI Flash programming
J63U9/U11 or U13 SPI Flash Programming SelectionRemovedEliminated in this revision
J64U10 or U12 SPI Flash Programming SelectionRemovedEliminated in this revision
J65CEC173x AP0_RESET# connect to MEC1723 RESET_IN#0 Ohm Short - R150IN (Default): Connect

OUT: Disconnect