6.1.8 SHA Command
The SHA command computes a SHA-256 or HMAC/SHA digest for
general purpose use by the host system. The SHA computation is performed in a special
section of internal ATECC608C-TFLXTLS memory (Context Buffer)
that is not read nor written by any other commands. Any arbitrary command can be
interspersed between the various phases of the SHA command without
problems. This SHA context is invalidated on power-up and wake. In most cases, if an
error occurs during the execution of the SHA command, the context is
retained without change.