3 EEPROM Memory and Data Zone Access Policies
The EEPROM memory contains a total of 1,400 bytes and is divided into the following zones:
| Zone | Description | Nomenclature |
|---|---|---|
| Configuration | Zone of 128 bytes (1,024
bits) EEPROM that contains:
| Config[a:b] = A range of bytes within a field of the Configuration zone |
| Data | Zone of 1,208 bytes (9.7 Kb) split into 16 general purpose read-only or read/write memory slots. The access policy information defined by the Configuration zone bytes determines how each slot can be accessed. The Access Policy for each data slot in the ATECC608C-TFLXTLS device has already been set and the slot Access Policies defined by the Configuration zone are in full effect. Some slots can be read from or written to while others cannot, depending upon that slot's Access Policy. | Slot[YY] = The entire contents stored in Slot YY of the Data zone |
| One-Time-Programmable (OTP) | Zone of 64 bytes (512 bits) arranged into two blocks of 32 bytes each. For the ATECC608C-TFLXTLS, the zone is preloaded with a predefined value. This zone cannot be modified but can be read at any time. See Section ATECC608C-TFLXTLS EEPROM One Time Programmable (OTP) Zone for more information. | OTP[bb] = A byte within the OTP zone, while OTP[aa:bb] indicates a range of bytes |
| Term | Meaning |
|---|---|
| Block | A single 256-bit (32-byte) area of a particular memory zone. The industry standard SHA-256 documentation also uses the term block to indicate a 512-bit section of the message input. Within this document, this convention is used only when describing hash input messages. |
| KeyID | KeyID is equivalent to the slot number for those slots designated to hold key values. Key 1 (sometimes referred to as key[1]) is stored in Slot[1] and so on. While all 16 slots can potentially hold keys, those slots that are configured to permit clear text reads are not normally used as private or secret keys by the crypto commands. |
| mode[b] | Indicates bit, b, of the parameter mode. |
| SRAM | Contains input and output buffers, as well as internal state storage locations. This memory is not directly accessible by the user. |
| Word | A single 4-byte word of data read from or written to a block. The word is the smallest unit of data access. |
| LSB/MSB | Least Significant Byte/Most Significant Byte. |
| LSb/MSb | Least Significant Bit/Most Significant Bit. |