2.5 Limit Switches
The Home section of this document describes how a limit switch is placed on both axes. The limit switches are used to help home (reset to the origin position) the platform before operation by advancing the platform in their direction until they are pressed. The switch is wired in the normally closed configuration and pulled low. This ensures the pin will be high even if the limit switch is tripped or if the limit switch is disconnected.