1.3 System Requirements
The M-HSM server can run on Windows 7 x64 Pro, Windows 8.1 x64 operating systems, or Windows 10 x64. Server software is installed on a dedicated physical machine with one nShield Edge or Solo HSM module attached.
Note: It is possible to use a virtual machine
to run the HSM server. However, Microchip has only validated M-HSM server functionality
on the nShield Edge module using a VMWare virtual machine. Validation was performed
using the nCipher-suggested method of connecting the Edge module directly to the host
system and then giving the virtual machine module access through a virtual COM interface
added to the host system by the module driver. See the nShield Edge and Solo User
Guide for Windows for setup instructions.