4.1.2 Update Service Properties
Perform the following steps to update service properties:
- Open the Control Panel and go to Services. Find the Manufacturer HSM Service entry and open the service properties windows.
- On the General tab, set
Startup type to Automatic (Delayed Start).

- On the Log On tab, make sure "Log On as" is set to Local System
account.

- On the Recovery tab, set all
failure recovery fields to Restart the Service, as shown in the following
figure. This setting tells Windows to automatically restart the server, if an error
occurs.

- When completed, click OK and
close the dialog box. Then, attempt to manually start the server: navigate to the
Manufacturer HSM Server entry, right-click, and choose Start.

- Once service is confirmed, you can reboot the PC and log in using a non-administrator user account.
Note: Under the non-administrator account, you can only observe service status using the
Windows Services tool.