5.7.2 Run the EEPROM Script
From the "%DIR_PATH%\SOFTWARE\" folder, launch the following command:
- SAM9X60D1G_EEprom_Check.bat
The following contents appear in the Command Prompt window and in the debug UART interface.
When the three tests are a pass, indicated by a ‘P’ as shown above, the connection between the two devices is confirmed.
If the test is stuck, the only way to return to a valid state is to perform a hardware reset by forcing the NRST signal to ground.
Important: This test erases all
data currently contained in the EEPROM memory.