1.8 DAC Waveform Generation with DMA
This example application shows how to use the DAC with the DMA to generate a 5 kHz sinusoidal waveform without CPU intervention.
Description
The DAC Peripheral library is used in hardware trigger mode to generate a Sine wave. The TC peripheral is configured to generate a trigger every two microseconds. Trigger is connected to the DAC using the EVSYS peripheral. DMA is used to setup a linked list to transfer sine wave samples from look up table to the DAC “DATABUF” register. In this application, the number of DAC samples per cycle(0 to 360 degrees sine wave) is 100.
Downloading and Building the Application
To clone or download this application from Github, go to the main page of this repository and then click Clone button to clone this repository or download as zip file. This content can also be downloaded using content manager by following these instructions.
Path of the application within the repository is apps/dac/dac_wav_gen_dma/firmware.
To build the application, refer to the following table and open the project using its IDE.
| Project Name | Description |
|---|---|
| sam_l21_xpro.X | MPLABX project for SAM L21 Xplained Pro Evaluation Kit |
Setting Up the Hardware
The following table shows the target hardware for the application projects.
| Project Name | Description |
|---|---|
| sam_l21_xpro.X | SAM L21 Xplained Pro Evaluation Kit |
Setting Up SAM L21 Xplained Pro Evaluation Kit
- Connect an oscilloscope to monitor the DAC pin PA05 (Pin 15 of the EXT1 header)
- Connect the Debug USB port on the board to the computer using a micro USB cable
Running the Application
- Build and Program the application using its IDE
- Observe a sine wave of 5 kHz frequency on DAC output pin
- Refer to the below table for DAC output pin details:
Board DACC Output Pin SAM L21 Xplained Pro Evaluation Kit PA05 (Pin 15 of the EXT1 header)