Edit the
OPAMP0_init() so it configures OP0 to be a voltage
follower
Plot the input and output of OP0 in the MPLAB® Data Visualizer
Edit
OPAMP0_init() to set the time base for the OPAMP
peripheral by writing:
OPAMP.TIMEBASE = OPAMP_TIMEBASE_US;
Info: For internal timing purposes, the Timebase (OPAMP.TIMBASE) register needs
the maximum number of CLK_PER cycles to achieve a timing interval equal to
or larger than 1 µs. The rule to determine what number to write into the
TIMBASE is: Determine the number of CLK_PER cycles equal to 1 µs. If this is
an integer, subtract one. If not, round it down. The following macro can be
used to calculate the value for the TIMEBASE register:
#defineOPAMP_TIMEBASE_US (ceil(F_CPU /1e6)-1)
Set the output mode to normal and
the Always On (ALWAYSON) bit for OP0 by writing:
Info: Each op amp instance in the OPAMP peripheral has an independent output
mode. The two modes are off and normal. In the off mode, the output driver
for the op amp is off but can be overwritten by the DRIVE event. In the
normal mode, the driver is always on.
Info: Each op amp
instance in the OPAMP peripheral can be individually turned on or off. This
can be achieved either by setting/clearing the ALWAYSON bit or by the
ENABLEn/DISABLEn events. If events are used to control the op amp, the
ALWAYSON bit has to be cleared.
Warning: The Event Enable (EVENTEN)
bit must be set in the OPnCTRA register to control the op amp using
events
Configure OP0 to be a voltage
follower with the DAC as an input by writing:
OPAMP.OP0INMUX = OPAMP_OP0INMUX_MUXNEG_OUT_gc | OPAMP_OP0INMUX_MUXPOS_DAC_gc;
/* Configure the Op Amp n Resistor Wiper Multiplexer */
OPAMP.OP0RESMUX = OPAMP_OP0RESMUX_MUXBOT_OFF_gc | OPAMP_OP0RESMUX_MUXWIP_WIP0_gc |
OPAMP_OP0RESMUX_MUXTOP_OFF_gc;
Info:Figure 5-1. Op Amp in Voltage
Follower ConfigurationTo achieve a voltage follower configuration, the output of the op amp
needs to be connected directly to the negative input. This is done by
setting the Multiplexer for Negative Input (MUXNEG) bit field in the Op Amp
n Input Multiplexer (OPnMUX) register to OUT. The output of the DAC and the
positive input to OP0 are connected through an internal channel by setting
the Multiplexer for Positive Input (MUXPOS) bit field in the OPnMUX register
to DAC. There is no need to use the resistor ladder in the voltage follower,
so all the bit fields in the Op Amp n Resistor Ladder Multiplexer
(OPnRESMUX) register can be set to their default values.
Set the settling time by writing:
OPAMP.OP0SETTLE = OPAMP_MAX_SETTLE;
Info: The value in the Op Amp n Settle Timer (OPnSETTLE) register is the number
of microseconds needed for the output of the op amp to settle. This time is
highly application dependent. If it is not known, it is recommended to set
it to the max value 0x7F. This value, together with the
value in the TIMEBASE register, is used by an internal timer to determine
when to generate the READYn event and set the SETTLED flag in the OPnSTATUS
register.
Enable the OPAMP peripheral by writing:
OPAMP.CTRLA = OPAMP_ENABLE_bm;
Wait for the op amp to settle
before leaving the initialization by checking the Op Amp has Settled (SETTLED)
bit field in the Op Amp n Status (OPnSTATUS)
register:
while (!(OPAMP.OP0STATUS & OPAMP_SETTLED_bm))
{
;
}
Verify that the solution/project builds by selecting
the Build → Build
Solution from the top menu
bare in Atmel Studio or by pressing the
F7 key.
Flash the device by selecting the Debug → Start without
debugging
from the top menu bar in Atmel Studio or by pressing the
Ctrl+Alt+F5 keys.
Result: The
device is now flashed and ready to start streaming data to the MPLAB® Data
Visualizer.