Open MPLAB® Mindi™, press File→Open or Ctrl+o, and
locate the file Non_Inverting_PGA.wxsch in the location where the zip
file was extracted.
Simulate by pressing the Run
Schematic button.
Result: If everything worked
correctly, the plot of the simulation, as shown in Figure 1,
should come up. Figure 6-1. Assignment 4:
MPLAB® Mindi™ Plot
Change the resistors R1_OP0 and R2_OP0 to the once corresponding to WIP3. This
will set the gain to 2x.
Simulate with the new resistor
values by pressing Run Schematic.
Result: The
plot in MPLAB® Mindi™ should look similar to the one in Figure 2, where the
red waveform is the output from the op amp, and the green is the input. As expected,
the output is twice as large as the input. Figure 6-2. Assignment 4: Mindi™ Result