43.6.5 Events
The TSENS can generate the following output event:
- Window Monitor (WINMON): Generated when the measurement results matches the window monitor condition. Refer to CTRLC43.8.3 Control C for details.
Writing a one to an Event Output bit in the Event Control Register (EVCTRL.WINEO) enables the corresponding output event. Writing a zero to this bit disables the corresponding output event. Refer to the Event System chapter for details on configuring the event system.
The TSENS can take the following action on an input event:
- Start measurement (START): Start a measurement. Refer to CTRLB43.8.2 Control B for details.
Writing a one to an Event Input bit into the Event Control register (EVCTRL.STARTEI) enables the corresponding action on input event. Writing a zero to this bit disables the corresponding action on input event. Refer to the Event System chapter for details. By default, the TSENS will detect a rising edge on the incoming event. If the TSENS action must be performed on the falling edge of the incoming event, the event line must be inverted first, by writing to one the corresponding Event Invert Enable bit in Event Control register (EVCTRL.STARTINV).