17.4.2.3 Write Access Protection Management Errors

Only word-wise writes to the Write Control (WRCTRL) register will effectively change the access protection. Other type of accesses will have no effect and will cause a PAC write access error. This error is reported in the Peripheral Interrupt Flag Status and Clear (INTFLAGA.PAC) bit.

PAC also offers an additional safety feature for correct program execution with an interrupt generated on double write clear protection or double write set protection. If a peripheral is write-protected and a subsequent set protection operation is detected, then the PAC returns an error, and similarly for a double clear protection operation.

In addition, an error is generated when writing a “set and lock” protection to a write-protected peripheral or when a write access is done to a locked set protection. This can be used to ensure that the application follows the intended program flow by always following a write-protect with an unprotect and the other way around. However, in applications where a write-protected peripheral is used in several contexts, e.g. interrupt, care must be taken so that either the interrupt can not happen while the main application or other interrupt levels manipulates the write protection status or when the interrupt handler needs to unprotect the peripheral based on the current protection status by reading the Peripheral Write Protection Status (STATUSn) register.

The errors generated while accessing the PAC module registers (for example, key error, double protect error, and so on) will set the Peripheral Interrupt Flag Status and Clear (INTFLAGA.PAC) bit.