6.2.1 Adding a Label to a Snapshot

After clicking a captured data file or snapshot, the data are plotted similar to Figure 6-5.

Figure 6-5. Snapshot Labeling Tools
???

Repeat the following steps for each data file that needs to be labeled:

  1. Click Create a New Segment (A).
  2. Select the range that a segment or label will cover from measured data. In this example, from start to end is selected (B).
    1. Use the created labels for each of the files captured, either normal_operation or unbalanced_load.
  3. Select the label that the segment will be represented by (C).
  4. Save the changes (D).