22.2.1 Capture Sources
The capture source is selected with the CTS bits.
In Capture mode, the CCPx pin must be configured as an input by setting the associated TRIS control bit.
Important: If the CCPx pin is configured as an output, a
         write to the port can cause a capture event.