1.4 Programming a Device
To program a device, follow these steps:
Note: Prior to handling ESD components, attach a grounding strap to your wrist and the antistatic connection on the side of the programmer.
- Click Device.
Figure 1-18. Device Selection Window 
- Select the intended device from the list.
Figure 1-19. Device and Data Pattern (Programming File) Selection - Click Data Pattern.
- To open a file, click Open.
- To search a file, click Browse.
- Select the file to load.
- Select the appropriate settings.
- Click Open.
- Click OK.
- Click OK.
Figure 1-20. Loading Programming File - On the Program tab, select the appropriate settings for device operations.
Figure 1-21. Program Tab - On the Quantity field, select the number of devices to program.
- Place the first device in the programming adapter module.
- Click Program.
- If the quantity field is set greater than one, on the SS4 programmer, press the START push button.
Figure 1-22. START Push Button - After the green Pass or red Fail LED is lit, place another device (if the quantity field is greater than 1) in the programming adapter module.
- On the programmer, press the START push button.
The following figure shows the output after programming the device.
Figure 1-23. Output—Programing Device