3.1 Using the Curiosity Nano AVR128DB48
To illustrate the capabilities of Multi-Voltage I/O an AVR128DB48 Curiosity Nano is used.
Schematics of the Curiosity Nano PCB can be found in the References section. To enable MVIO on this development board,
perform the below steps:
- Remove the resistor right below the VDDIO2 label to disconnect VDDIO2 from VDD. This is resistor R204 in Figure 3-2.
- Connect VDDIO2 + to 3.3V of a second power voltage source.
- Connect VDDIO2 - to GND of a second voltage source.
Refer to the AVR123DB48 Curiosity Nano User Guide for a guide on how to reverse this process.
Any voltage between 1.8V and 5.5V may be applied to VDDIO2, but for the following examples, we will run at 3.3V.