Introduction
| Author: Victor Berzan, Microchip Technology Inc. |
The Analog-to-Digital Converter (ADC) peripheral converts an analog voltage to a numerical value. This peripheral is included in many AVR® microcontrollers (MCUs). A 10-bit single-ended ADC peripheral is available on most of the tinyAVR® and megaAVR® MCUs, while on the AVR DA family there is a 12-bit differential and single-ended ADC peripheral available.
- ADC
Single Conversion:
Initialize the ADC, start conversion, wait until the conversion is done, and read the ADC result.
- ADC
Free-Running:
Initialize the ADC, enable Free-Running mode, start conversion, wait until the conversion is done, and read the ADC result in an infinite loop.
- ADC
Sample Accumulator:
Initialize the ADC, enable accumulation of 64 samples, start conversion, wait until the conversion is done, and read the ADC result in a loop.
- ADC
Window Comparator:
Initialize the ADC, set the conversion window comparator low threshold, enable the conversion Window mode, enable the Free-Running mode, start the conversion, wait until the conversion is done and read the ADC result in an infinite loop, and light-up an LED if the ADC result is below the set threshold.
- ADC Event
Triggered:
Initialize the ADC, initialize the Real-Time Counter (RTC), configure the Event System (EVSYS) to trigger an ADC conversion on RTC overflow, toggle an LED after each ADC conversion.