An ADC conversion can be triggered by an event. This is enabled by writing a
‘1’ to the Start Event Input (STARTEI) bit in the Event Control
(ADCn.EVCTRL) register.Figure 7-1. ADC0.EVTRL - Enable the
STARTEI Bit
ADC0.EVCTRL |= ADC_STARTEI_bm;
Any incoming event routed to the ADC through the Event System (EVSYS) will
trigger an ADC conversion. The event trigger input is edge sensitive. When an event
occurs, STCONV in ADCn.COMMAND is set. STCONV will be cleared when the conversion is
complete.
For example, to start the ADC conversion on RTC overflow, the following settings must be
made:
The RTC overflow event must be
linked to channel 0 of the Event System.
The Event User ADC0 must be
configured to take its input from channel 0.
The STARTEI bit in the EVCTRL
register of the ADC must be set to enable the ADC conversion to be triggered by
events.
EVSYS.CHANNEL0 = EVSYS_GENERATOR_RTC_OVF_gc; /* Real Time Counter overflow */
EVSYS.USERADC0 = EVSYS_CHANNEL_CHANNEL0_gc; /* Connect user to event channel 0 */
ADC0.EVCTRL |= ADC_STARTEI_bm; /* Enable event triggered conversion */
Tip: The full code example is
also available in the Appendix section.
An MCC generated code example for AVR128DA48, with the same functionality as the one
described in this section, can be found here:
The online versions of the documents are provided as a courtesy. Verify all content and data in the device’s PDF documentation found on the device product page.