The simplest mode of using the ADC is to make a single conversion. The ADC input pin
needs to have the digital input buffer and the pull-up resistor disabled, to have the
highest possible input impedance. Pin PD6/AIN6 is used for ADC input in this
example.Figure 3-1. ADC0.MUXPOS Selection
ADC0.MUXPOS = ADC_MUXPOS_AIN6_gc;
The ADC Clock Prescaler can be used to divide the clock frequency. In this particular
example, the clock is divided by 4. The ADC can use VDD, external reference,
or internal reference for its positive reference. The internal reference is used in this
example.Figure 3-2. ADC0.CTRLC Voltage Reference
Selection
The ADC resolution is set by the RESSEL bit in the ADC0.CTRLA register. The
ADC is enabled by setting the ENABLE bit in the ADC0.CTRLA register.Figure 3-3. ADC0.CTRLA Resolution
Selection
The ADC conversion is started by setting the STCONV bit in the ADC0.COMMAND
register.Figure 3-4. ADC0.COMMAND - Start
Conversion
ADC0.COMMAND = ADC_STCONV_bm;
When the conversion is done, the RESRDY bit in the ADC0.INTFLAGS gets set by
the hardware. The user must wait for that bit to get set before reading the ADC
result.Figure 3-5. ADC0.INTFLAGS - Hardware-Set
RESRDY Bit
while (!(ADC0.INTFLAGS & ADC_RESRDY_bm))
{
;
}
The user must clear the RESRDY bit by writing ‘1’ to it
before starting another
conversion.
ADC0.INTFLAGS = ADC_RESRDY_bm;
The conversion result can be read from the ADC0.RES
register.
adcVal = ADC0.RES;
Tip: The full code example is
also available in the Appendix section.
An MCC generated code example for AVR128DA48, with the same functionality as the one
described in this section, can be found here:
The online versions of the documents are provided as a courtesy. Verify all content and data in the device’s PDF documentation found on the device product page.