2.1.2 LORAWAN_Reset
Definition: This function automatically resets the LoRaWAN stack software and initializes the stacks with the parameters for the selected ISM band. During this Reset routine:
- MAC DB is initialized with default parameters
- LoRaWAN regional parameters module is initialized
- Radio layer default DB initialization is triggered
The Reset routine must be called after every software reset of the stack. To change the regional band dynamically, Reset routine calls the new ISM band, which un-initializes an old regional parameter and re-initiates the new ISM band. If the ISM band is same as the one stored in DB, the regional parameter initializes the same default ISM band.
Syntax
StackRetStatus_t LORAWAN_Reset (IsmBand_t ismBand);
Input Parameters
|
Parameter Name |
Parameter Type |
Description |
|---|---|---|
|
| ISM band types. Refer to Table 2-37 for a list of defined ISM band types. |
Return Type and Values
|
Parameter Name |
Parameter Type |
Description |
|---|---|---|
|
|
ENUM |
Enumerated values containing all return types from LoRaWAN layers |
|
Return Value |
Reason |
|---|---|
|
|
LoRaWAN stack is successfully being reset and default values are restored |
|
|
Given ISM band is invalid |
API Type – Synchronous