8.3.2 IAR Settings
The compiler, linker, and assembler settings shown below are required while configuring for a specific device in IAR.
- When using the mEDBG in the
ATmega328PB Xplained Mini kit, the Atmel-ICE should be selected in Debugger Driver
setting (as shown in the figure below).
Figure 8-6. Debugger Driver
- A user-defined .xcl file should be
used to override default linker file. Follow the steps below to make the linker work
properly:
- Copy the template linker file (for example, C:\Program Files (x86)\IAR Systems\Embedded Workbench 7.4\avr\src\template\cfgm328pb.xcl) according to the device to your project and rename it what you like.
- Open this file and paste the
below content under the original content and save
it.
-ca90 -w29 //============================================================================= // Interrupt vectors -Z(CODE)INTVEC=BOOT_START-(BOOT_START+_..X_INTVEC_SIZE-1) //-H1895 -h(CODE)BOOT_START-(BOOT_START+_..X_INTVEC_SIZE-1) //============================================================================= // Code memory -Z(CODE)NEAR_F,HUGE_F,SWITCH,INITTAB,DIFUNCT,CODE=BOOT_START-_..X_FLASH_END -Z(FARCODE)FAR_F,FARCODE=BOOT_START-_..X_FLASH_END //============================================================================= // RAM -Z(DATA)NEAR_I,NEAR_Z=_..X_SRAM_BASE-_..X_SRAM_END -Z(DATA)RSTACK+_..X_RSTACK_SIZE=(_..X_SRAM_END-_..X_RSTACK_SIZE+1)-_..X_SRAM_END -Z(DATA)CSTACK+_..X_CSTACK_SIZE=(_..X_SRAM_END-_..X_RSTACK_SIZE-_..X_CSTACK_SIZE+1)-(_..X_SRAM_END-_..X_RSTACK_SIZE) //-Z(DATA)RSTACK+40=(_..X_SRAM_END-40+1)-_..X_SRAM_END //-Z(DATA)CSTACK+300=(_..X_SRAM_END-40-300+1)-(_..X_SRAM_END-40) //-Z(DATA)TINY_I,TINY_Z,TINY_N=RAM_BASE-FF //-Z(DATA)TINY_I,TINY_Z,TINY_N=RAM_BASE-100 - Use this file to override the
default linker file (as shown in the figure below).
Figure 8-7. Override Default Linker File
- Define BOOT_START (refer to
Table 8-1) according to the device (as shown in the
figure below).
Figure 8-8. Linker #define
- Optimization Settings (as shown in
the figure below).
Figure 8-9. Optimization Settings