3.3.4 How to Implement the Function that Handles STDIO
The function that handles STDIO is void puthc(char c).
Implementing this function will transmit its char argument over EUSART and will cause
the printf to be redirected to EUSART.
void putch(char txData)
{
EUSART2_write(txData);
}The following line will send messages over EUSART:
printf("%c%c%c%c", START_DATA_STREAM_PROTOCOL, cnt, cnt * 2, STOP_DATA_STREAM_PROTOCOL);The Data Stream Protocol frame has start and stop tokens, as inverse/one’s complement each other. In between those, the payload may contain any number of values. The protocol must be sent in binary format.
printf function
uses placeholder specifiers in the format string to mark where to insert variables. Some
of the available placeholders are displayed in the table below.| Placeholder | Description |
|---|---|
| %d | Insert a signed integer |
| %f | Insert a floating point number |
| %s | Insert a sequence of characters |
| %c | Insert a character |
| %x | Insert integer unsigned in hex
format |
In this example, the %c specifier is used, because the row binary value will be transmitted.
Use MPLAB X Data Visualizer as described in the appendix, How to Configure MPLAB X Data Visualizer to Decode Data Stream Protocol.