8.6 PICkit Basic Tool Options
Options specifically for the PICkit Basic tool.
| Programming mode entry | Use low voltage programming mode entry - always selected PICkit Basic does not support the high voltage Vpp option for placing the target device in programming mode and only supports the low voltage method (Vpp will not exceed the Vdd supply voltage. Instead a test pattern will be used on Vpp). |
| Program Speed | Select the speed the debugger will use to program the target as either Low, Normal or High. The default is Normal. If programming should fail, using a slower speed may solve the problem. |