8.2 Debugger Options Selection
Debugger options are set in the Project Properties dialog of MPLAB® X IDE. Click on PKB under Categories to display the Options for PKB (see figure below). Use the Options categories drop-down list to select various options. Click on an option name to see its description in the Option Description box below. Click to the right of an option name to select or change it.
After setting the options, click Apply or OK. Also click the
Refresh Debug Tool icon
in
the MPLAB X IDE dashboard display to update any changes made.
For the MPLAB IPE, the options for MPLAB PICkit Basic are located in . Refer to MPLAB IPE online help for more information.