Silicon Issue Summary
| Module | Feature | Item No. | Issue Summary | Affected Revisions | |
|---|---|---|---|---|---|
| A2 | A3 | ||||
| Analog-to-Digital Converter (ADC) | ADC Conversion | ADC Conversion | Delay of one instruction cycle required prior to setting the ADGO bit when using ADCRC as the ADCC clock source. | X | |
|
ADCRC Oscillator Operation in Sleep | ADCRC Oscillator Operation in Sleep | The ADCRC oscillator does not stop after conversion is complete in Sleep mode. | X | X | |
| ADC Conversion with FVR | Missing Codes with FVR Reference | Using FVR as the ADC positive voltage reference can cause missing codes. | X | X | |
| ADC Conversion with FOSC as Clock | ADC GO Bit May Remain Set When the Clock Source is FOSC | The ADGO bit remains set when using FOSC as clock source with clock divider. | X | X | |
| ADC Operation in Burst Average Mode | ADCC Burst Average Mode | The ADCNT register does not increment past ’0b1’ in Burst Average mode with double sampling enabled. | X | X | |
| Double Sample Conversions | Double Sample Conversions | An unexpected acquisition time is added between the first and second conversions. | X | X | |
| ADC Acquisition Time | ADC Conversion Acquisition Time in Sleep (ADCC) | Conversion during SLEEP mode when ADACQ=0 affects results on values in the upper half of the 10-bit range. The analog input is disconnected for 3-4 uS and the first bit of the result becomes zero. | X | X | |
| ADC Short in Pre-Charge State | ADC Short in Pre-Charge State | ADC shorts briefly in pre-charge state when the corresponding analog pin is selected as an output. | X | X | |
| PIC18 Debug Executive | Data Write Match Breakpoints | Data Write Match Breakpoints | Data write match breakpoints do not work when used on a location GSR space. | X | |
| Single Step Function (SSTEP) | Single Step Function Does Not Execute at SW Breakpoint | Single Step function does not execute at SW Breakpoint. | X | X | |
| PIC18 Core | TBLRD | TBLRD Requires NVMREG Value to Point to Appropriate Memory | TBLRD requires NVMREG value to point to appropriate memory. | X | |
| Program Flash Memory (PFM) | Endurance of PFM Cell | Endurance of PFM is Lower than Specified | Endurance of the PFM cell is lower than specified. | X | X |
| Back to Back Writes | PFM Back-to-Back Writes | Repetitive writes may cause write/erase failures. | X | X | |
| MSSP | SMBus 2.0 Voltage Level | SMBus 2.0 Voltage Level | Input low-voltage threshold level is dependent on VDD. | X | X |
| SPI | MSSP SPI Client Mode | SSPBUF may become corrupted. | X | X | |
| I2C | SMBus 2.0 Voltage Level | Acknowledge failure on LF devices only. | X | ||
| Electrical Specifications | Min VDD Specification | Min VDD Specification (LF Devices Only) |
VDDMIN specifications are changed for LF devices only for -40°C and 0°C. | X | |
| FVR Specification | FVR - Fixed Voltage Reference | FVR specifications require use above -20°C. | X | X | |
| Analog-to-Digital Converter | ADC - Analog-to-Digital Converter | ADC offset error specification is +/- 3.0 LSb. | X | X | |
| Timer0 | Synchronous Mode | Synchronous Mode | TMR0 does not function properly in Sync mode. | X | X |
| Clock Source | TMR0H Register Does Not Increment | TMR0H register does not increment when the clock source is Fosc/4 and the T0ASYNC bit is cleared. | X | X | |
| Windowed Watchdog Timer (WWDT) | WWDT Operation in Doze Mode | Window Operation in Doze Mode | Erroneous window violation error occurs in Doze mode. | X | X |
| Nonvolatile Memory (NVM) | NVMERR Bit Operation | NVMERR | NVMERR bit is set incorrectly due to specific Reset events. | X | X |
| Signal Measurement Timer (SMT) | Reset bit | Reset Bit | Module stops working if RST is set while prescaler setting is not zero. | X | X |
| Enhanced Universal Synchronous Asynchronous Receiver Transmitter (EUSART) | Transmit Mode | Double Byte Transmit | Possible duplicate byte transmitted. | X | X |
| Capture/Compare/PWM Module (CCP) | PWM Mode | Wrong Duty Cycle for CCP Module | Duty cycle values are incorrect. | X | X |
| In-Circuit Serial Programming™ | Low-Voltage Programming | Low-Voltage Programming Not Possible | Low-Voltage Programming is not possible when VDD is below BORV while BOR is enabled. | X | X |
|
Note:
Only those issues indicated in the last column
apply to the current silicon revision.
| |||||