4.4 GetInstalledCertificateIds
The GetInstalledCertificateIds message is used by the central system to request a list of the IDs of all certificates that are currently installed on the charge point. This helps the central system verify and manage the certificates being used for secure communication.
|
API Syntax |
Description |
Input Params |
Return Value |
|---|---|---|---|
IsInstalledCertificateAvailable | This function checks the availability of an installed certificate. It returns true. | void | bool |
Example:
if (IsInstalledCertificateAvailable())
{
LogDebug("APP_LOG", "GetInstalledCertificateIds: Certificate found and accepted\n");
SetInstalledCertificateStatus(INSTALLED_CERTIFICATE_ACCEPTED);
}
|
API Syntax |
Description |
Input Params |
Return Value |
|---|---|---|---|
SetInstalledCertificateStatus |
This function updates the status of the installed certificate. The status is passed as an enumerated value, which indicates the current state of the certificate installation process. | GET_INSTALLED_CERT_STATUS_T status | void |
Example:
if (IsInstalledCertificateAvailable())
{
LogDebug("APP_LOG", "GetInstalledCertificateIds: Certificate found and accepted\n");
SetInstalledCertificateStatus(INSTALLED_CERTIFICATE_ACCEPTED);
}
|
API Syntax |
Description |
Input Params |
Return Value |
|---|---|---|---|
SendGetInstalledCertificateIdsResponse | This function sends the response for the GetInstalledCertificateIds request. | char *resUUID | GET_INSTALL_ERR_T |
Example:
if (IsInstalledCertificateAvailable())
{
LogDebug("APP_LOG", "GetInstalledCertificateIds: Certificate found and accepted\n");
SetInstalledCertificateStatus(INSTALLED_CERTIFICATE_ACCEPTED);
}
else
{
LogDebug("APP_LOG", "GetInstalledCertificateIds: Certificate not found\n");
SetInstalledCertificateStatus(INSTALLED_CERTIFICATE_NOT_FOUND);
}
SendGetInstalledCertificateIdsResponse(messageID);
|
API Syntax |
Description |
Input Params |
Return Value |
|---|---|---|---|
ConvertToHex | Function to convert the string to hexadecimal format | char *input, int length, char *output | static void |
Example:
OCSP_id_get0_info(&issuerNameHash, NULL, &issuerKeyHash, &serial, cid);
ConvertToHex(ASN1_STRING_get0_data(issuerNameHash), ASN1_STRING_length(issuerNameHash), certHashData->issuerNameHash);
ConvertToHex(ASN1_STRING_get0_data(issuerKeyHash), ASN1_STRING_length(issuerKeyHash), certHashData->issuerKeyHash);
ConvertToHex(ASN1_STRING_get0_data(serial), ASN1_STRING_length(serial), certHashData->serialNumber);