3.8.5 Ping Demo
This application demonstrates how a user can run a ping test on WINC1500 device.
Configure the wifi parameters using "wifi set" command.

Enter the command "sping <ip_address> <no_of_ping>".

Then enter the command "appdemo start 1 9" to run the Ping demo. First the device will connect to the network. After the IP address has displayed on the terminal window, the ping command will start.