1.5.2 PFM Back to Back Writes
When repetitive writes to non-volatile memory (Program Flash Memory) are performed, it could result in write/erase failures at some locations. The issue is due to latent timing in the non-volatile memory controller which can cause the write instruction to fail under certain conditions.
Work around
To avoid the issue, the customer needs to wait an additional 100 us after the NVMCON1.WR bit has been set, allowing for the last word to be loaded into the latch. This delay is added only when the NVMCON1.LWLO bit is cleared in the software.
if(i == (WRITE_FLASH_BLOCKSIZE-1))
{
// Start Flash program memory write
NVMCON1bits.LWLO = 0;
}
NVMCON2 = 0x55;
NVMCON2 = 0xAA;
NVMCON1bits.WR = 1;
if (NVMCON1bits.LWLO==0)
{
__delay_us(100);
}
NOP();
NOP();
writeAddr++;
}
Affected Silicon Revisions
| A0 | A1 |
| X |