2.3.3 Debugging a Device
Use the following commands to debug a device.
- Reset – refer to the device data sheet for Reset information. If a Reset is
needed for debugging purposes: first, halt the target; then, enter the
command:
Reset - Set Breakpoint – there are two ways to set a breakpoint for debugging:
Set a breakpoint by source-line-number using the command:
Break filename: linenumberFor example:
Break main.c:53Set a breakpoint at an absolute address using command:
Break *addressFor example:
Break *0x108 - Set Watchpoint – to set a watchpoint for debugging:
Set a watchpoint by specifying an address and the type of watch using the command:
Watch address breakontypeFor example:
Watch 0xa0007ff0 Ror
Watch address breakontype[:value] [passcount]For example:
Watch 0xa0007ff0 R:0xf 1 - Delete Breakpoint – to delete
a breakpoint, use the command:
Delete [breakpoint number]If no argument is specified in this command, it will delete all breakpoints.
- Run Program – the Run command can be used to run the program until it reaches a breakpoint.
- Step Through – to step through the program, use the Step command or Next command.
- See Variable Value – a Print [variable] command can be used to see the value of a variable or an SFR.
- Exit – use the Quit command to exit the MDB.