2.3.1 Entering Commands Method
Note: Although the MPLAB X IDE can run
multiple tools simultaneously, the MDB will run only one tool at a time. However, you
can have multiple instances of the MDB running. Refer to Using Multiple Instances of the MDB for details.
Entering commands is a step-by-step method to run a test with MDB. Once the MDB is running, you can start entering commands. Note that while the MDB commands are not case-sensitive, the property options and file names are case-sensitive.
Type help for a list of classes of commands in MDB. Refer to MDB Reference, Table 3-1.
For other commands available, see MDB Reference, Table 2-2 through Table 2-10.
The following sections describe these topics:
- Programming a Production Image for Testing Purposes
- Debugging a Device