20.14.4 ANSELx

Analog Select Register
Important:
  • When setting a pin as an analog input, the corresponding TRIS bit must be set to Input mode to allow external control of the voltage on the pin
  • Refer to the “Pin Allocation Table” for details about pin availability per port
  • Unimplemented bits will read back as ‘0’
Name: ANSELx

Bit 76543210 
 ANSELx7ANSELx6ANSELx5ANSELx4ANSELx3ANSELx2ANSELx1ANSELx0 
Access R/WR/WR/WR/WR/WR/WR/WR/W 
Reset 11111111 

Bits 0, 1, 2, 3, 4, 5, 6, 7 – ANSELxn Analog Select on RX Pin

ValueDescription
1 Analog input. Pin is assigned as analog input. Digital input buffer disabled.
0 Digital I/O. Pin is assigned to port or digital special function.
When setting a pin as an analog input, the corresponding TRIS bit must be set to Input mode to allow external control of the voltage on the pin Refer to the “Pin Allocation Table” for details about pin availability per port Unimplemented bits will read back as ‘0’