1.20 SST26 SQI Flash Driver - Flash read write in SPI mode
This example application shows how to use the SST26 driver to perform block operations on the On-Board SST26 Flash memory in SPI mode.
Description
This application uses the SST26 driver to Erase/Write/Read on the On-Board SST26 Flash memory using the SQI peripheral library configured in SPI mode. The application consists of APP_SST26_Tasks() which is called through SYS_Tasks() routine.
Downloading and Building the Application
To clone or download this application from Github, go to the main page of this repository and then click Clone button to clone this repository or download as zip file. This content can also be downloaded using content manager by following these instructions.
Path of the application within the repository is apps/driver/sqi_flash/sst26/sst26_spi_read_write/firmware.
To build the application, refer to the following table and open the project using its IDE.
| Project Name | Description |
|---|---|
| sama5d29_curiosity.X | MPLABX project for SAMA5D29 Curiosity Development Board |
Setting Up AT91Bootstrap loader
To load the application binary onto the target device, we need to use at91bootstrap loader. Refer to the at91bootstrap loader documentation for details on how to configure, build and run bootstrap loader project and use it to bootstrap the application binaries.
Setting Up the Hardware
The following table shows the target hardware for the application projects.
| Project Name | Description |
|---|---|
| sama5d29_curiosity.X | SAMA5D29 Curiosity Development Board |
Setting Up SAMA5D29 Curiosity Development Board
- Connect the SQI Boot Jumper (J10).
- Connect the Debug USB port on the board to the computer using a USB-C cable
Running the Application
- Build the application using its IDE
- LED is turned ON when the data read from SST26 flash matches with the data written in it
| Board | LED Name |
|---|---|
| SAMA5D29 Curiosity Development Board | RGB_LED (Green) |