1.1 FAT Filesystem throughput using SDMMC Media

This application calculates throughput by Writing and Reading data into a SD-Card at High Speed using the MPLAB Harmony File System and the SDMMC driver.

Description

Application performs below filesystem operations and throughput calculations on SD-Card using both Aligned and Unaligned buffers

  • Opens a file named throughput.txt in the root directory of the SD card.
  • Writes 10 Megabytes of data to file in chunks of 64 Kilobytes.
  • Once the operation is completed it calculates the time taken and overall throughput for write in Megabytes/second and displays on the console.
  • Reads 10 Megabytes of data from file in chunks of 64 Kilobytes.
  • Once the operation is completed it calculates the time taken and overall throughput for reading in Megabytes/second and displays on the console.
  • Closes the file once read is completed.
  • Checks if the Above steps need to be repeated for Unaligned buffer. If already done then it Glows an LED reporting success and the console will have throughput information for both Aligned and Unaligned buffers.

File system layer uses:

  • SDMMC Driver to communicate to SD Card

Downloading and Building the Application

To clone or download this application from Github, go to the main page of this repository and then click Clone button to clone this repository or download as zip file. This content can also be downloaded using content manager by following these instructions.

Path of the application within the repository is apps/fs/sdmmc_fat_throughput/firmware.

To build the application, refer to the following table and open the project using its IDE.

Project NameDescription
sama5d29_curiosity.XMPLABX project for SAMA5D29 Curiosity Development Board

Setting Up AT91Bootstrap loader

To load the application binary onto the target device, we need to use at91bootstrap loader. Refer to the at91bootstrap loader documentation for details on how to configure, build and run bootstrap loader project and use it to bootstrap the application binaries.

Setting Up the Hardware

The following table shows the target hardware for the application projects.

Project NameDescription
sama5d29_curiosity.XSAMA5D29 Curiosity Development Board

Setting Up SAMA5D29 Curiosity Development Board

ADDTIONAL HARDWARE REQUIRED
  • SD Card with FAT32 file system
    • The SD Card should have at least 10MB of free space for the demo to work
SETTING UP THE BOARD
  • Insert the SD card into Micro-SD Card slot (J6) provided under the board.
  • Connect the Debug USB port on the board to the computer using a USB-C type cable
  • Connect UART Debug port on board to the computer using FTDI-USB cable.

Running the Application

  1. Build the application using its IDE.
  2. Open the Terminal application (Ex.:Tera term) on the computer.
  3. Connect to the Virtual COM port and configure the serial settings as follows:
    • Baud : 115200
    • Data : 8 Bits
    • Parity : None
    • Stop : 1 Bit
    • Flow Control : None
  4. The LED is turned ON if there was no error during the file operations.
    Refer to the following table for LED name:
    BoardLED Name
    SAMA5D29 Curiosity Development BoardRGB_LED (Green)
  5. Calculated throughput values for Aligned and Un-aligned buffers are displayed on console as below:
    Note: The Values showed in the below output may differ slightly when demo is run.

Additional Steps (Optional)

To increase the throughput for the Un-aligned buffers you can follow below steps

  • Launch MCC for the project.
  • Increase the size for the internal aligned buffer used by Filesystem service with some value as shown below. This internal buffer will be used when application buffer is Un-aligned and placed in cacheable region.
  • Note: Increasing the size of the aligned buffer will consume more RAM.
  • Regenerate the project.
  • Once done repeat the steps mentioned in Running the Application and observe the change in throughput for Un-aligned buffer.