1.3 FAT Filesystem using SQI Flash Media
This application shows an example of using the MPLAB Harmony File System to access SQI based flash media. The SAMA5D29 Curiosity Development Board, SAMA5D27-SOM1-EK1 and the SAMA5D27-WLSOM1-EK1 have the SST26 flash media.
Description
File System Operations on the On-Board SQI Flash Memory
- Performs a SYS_FS_FormatDisk
- Opens a newfile.txt on the flash memory
- Write and reads back 4KB of data on newfile.txt
- Verifies the Data Read back
File system layer uses the following components:
- One instance of the Memory driver is used to communicate with the On-Board SQI Flash memory
Downloading and Building the Application
To clone or download this application from Github, go to the main page of this repository and then click Clone button to clone this repository or download as zip file. This content can also be downloaded using content manager by following these instructions.
Path of the application within the repository is apps/fs/sqi_flash_fat/firmware.
To build the application, refer to the following table and open the project using its IDE.
| Project Name | Description |
|---|---|
| sama5d29_curiosity.X | MPLABX project for SAMA5D29 Curiosity Development Board |
| sama5d29_curiosity_freertos.X | MPLABX project for SAMA5D29 Curiosity Development Board |
| sam_a5d27_som1_ek_freertos.X | MPLABX project for SAMA5D27-SOM1-EK1 |
| sam_a5d27_wlsom1_ek1_freertos.X | MPLABX project for SAMA5D27-WLSOM1-EK1 |
Setting Up AT91Bootstrap loader
To load the application binary onto the target device, we need to use at91bootstrap loader. Refer to the at91bootstrap loader documentation for details on how to configure, build and run bootstrap loader project and use it to bootstrap the application binaries.
Setting Up the Hardware
The following table shows the target hardware for the application projects.
| Project Name | Description |
|---|---|
| sama5d29_curiosity.X | SAMA5D29 Curiosity Development Board |
|
sama5d29_curiosity_freertos.X | SAMA5D29 Curiosity Development Board |
| sam_a5d27_som1_ek_freertos.X | SAMA5D27-SOM1-EK1 |
| sam_a5d27_wlsom1_ek1_freertos.X | SAMA5D27-WLSOM1-EK1 |
Setting Up SAMA5D29 Curiosity Development Board
- Connect the SQI Boot Jumper (J10)
- Connect the USB_A port on board to the computer using a USB-C type cable.
Setting Up SAMA5D27-SOM1-EK1
- Connecting a micro-USB cable to J10 both powers the board as well as provides a virtual COM port to open a serial terminal
Setting Up SAMA5D27-WLSOM1-EK1
- Connect a USB to UART FTDI cable to J26 (DEBUG FTDI) to open a serial terminal
- Connecting a micro-USB cable to J10 powers the board
- Press the SW3 (nSTART_SOM) button to power the ATSAMA5D27-WLSOM1 System-On-Module
- Make sure to disconnect the Jumper J8 (disable boot pin)
Running the Application
- Build the application using its IDE
- The LED is turned ON if data has successfully been written and read back from file “newfile.txt”
| Board | LED Name |
|---|---|
| SAMA5D29 Curiosity Development Board | RGB_LED (Green) |
| SAMA5D27-SOM1-EK1 | D5 (Green) |
| SAMA5D27-WLSOM1-EK1 | LD1 (Green) |